K65F180M Not Availble Device.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K65F180M Not Availble Device.

ソリューションへジャンプ
1,951件の閲覧回数
echris
Contributor III

I am trying to create a new Kinetis project, but my board is not listed under 'Devices'.  I am trying to find the K65F180M or TWR-K65F180M, yet it does not appear on the list.

 

What am I missing?

 

Thanks for the help.

ラベル(1)
1 解決策
1,843件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Eric,

I think you have not installed the Kinetis SDK v1.3?

Download and install the Kinetis SDK from http://www.freescale.com/ksdk, then in KDS install the update from C:\Freescale\KSDK_1.3.0\tools\eclipse_update with Help > Install New software and pointing to the .zip file there.

I hope this helps,

Erich

元の投稿で解決策を見る

2 返答(返信)
1,844件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Eric,

I think you have not installed the Kinetis SDK v1.3?

Download and install the Kinetis SDK from http://www.freescale.com/ksdk, then in KDS install the update from C:\Freescale\KSDK_1.3.0\tools\eclipse_update with Help > Install New software and pointing to the .zip file there.

I hope this helps,

Erich

1,843件の閲覧回数
echris
Contributor III

That worked perfectly.  Thanks.

0 件の賞賛
返信