K-64 Unable to Connect to GDBserver for Debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K-64 Unable to Connect to GDBserver for Debug

17,240 Views
Designer11
Contributor IV

Hi All,

I'm having issue with KDS connecting to the gdbserver for debugging in KDS IDE after my computer is reset. Initially, I was able to have connection between KDS and gdbserver and debug the code without any issue.  However, after i reset my computer,  KDS keep hanging  at 60 percent whenever i try to enter debug mode.

To verify whether there is still connection between my computer and the target i used SEGGER J-Link GDB server GUI  and commander and  noticed that the debugger probe is indeed connected to the K-64 MCU but not to the GDBServer, waiting for connection to GDB is the message i received.

I also attached a few images of the project setting in KDS  for Segger debug probe that used to work and now failed.

What i did but didn't help solve the issue:

-------------------------------------------------------

-Reset and turn off the computer

-Removed all breakpoints

-Power cycled the target/host and debug probe

-Switched to using PEMicro Multilink

-Switched to using another laptop

-Created new workspace, and test project

Questions:

- Should I talk to IT to open certain ports or allow certain IP range ?

Thank you in advance for the help.

Vu

Tags (3)
0 Kudos
Reply
7 Replies

16,170 Views
Designer11
Contributor IV

Hi Erich and Marcelo,

I got this issue  resolved after i uninstalled and  installed the latest Kinetis Design Studio from NXP to get it to work reliably. Keep my fingers crossed. 

Thanks,

Vu

0 Kudos
Reply

16,170 Views
mvaranda
Contributor I

MCUXpresso is VERY unstable. I am able to debug my app until I get a random "unrecoverable" unable to connect situation. The only way it resumes working is if I use Segger JTAG via IAR IDE. Then I can close IAR and restart MCUXpresso IDE and it may work for a while until stop working once again.

Logs from Windows 10 machine:

  SEGGER J-Link GDB Server V6.20g Command Line Version
  JLinkARM.dll V6.20g (DLL compiled Oct 20 2017 17:09:27)
  Command line: -nosilent -swoport 2337 -select USB=203200565 -telnetport 2338 -singlerun -endian little -noir -speed auto -port 2339 -vd -device MK66FN2M0xxx18 -if SWD -halt -reportuseraction
  -----GDB Server start settings-----
  GDBInit file:                  none
  GDB Server Listening port:     2339
  SWO raw output listening port: 2337
  Terminal I/O port:             2338
  Accept remote connection:      localhost only
  Generate logfile:              off
  Verify download:               on
  Init regs on start:            off
  Silent mode:                   off
  Single run mode:               on
  Target connection timeout:     0 ms
  ------J-Link related settings------
  J-Link Host interface:         USB
  J-Link script:                 none
  J-Link settings file:          none
  ------Target related settings------
  Target device:                 MK66FN2M0xxx18
  Target interface:              SWD
  Target interface speed:        auto
  Target endian:                 little
  Connecting to J-Link...
  J-Link is connected.
  Device "MK66FN2M0XXX18" selected.
  Firmware: J-Trace Cortex-M Rev.3 compiled May 22 2017 18:32:06
  Hardware: V3.10
  S/N: 203200565
  Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB
  Checking target voltage...
  Target voltage: 3.31 V
  Listening on TCP/IP port 2339
  Connecting to target...InitTarget()
  Found SW-DP with ID 0x2BA01477
  Scanning AP map to find all available APs
  AP[2]: Stopped AP scan as end of AP map has been reached
  AP[0]: AHB-AP (IDR: 0x24770011)
  AP[1]: JTAG-AP (IDR: 0x001C0000)
  Iterating through AP map to find AHB-AP to use
  AP[0]: Skipped. Invalid implementer code read from CPUIDVal[31:24] = 0x00
  AP[1]: Skipped. Not an AHB-AP
  InitTarget()
  Connect Under Reset
  Communication error while accessing MDM-AP.
  Connect Under Reset
  ERROR: Could not find core in Coresight setup
  Communication timed out: Requested 20 bytes, received 0 bytes !
  Could not transfer JTAG data.
  InitTarget(): PCode returned with error code -1
  ERROR: Could not connect to target.
  Target conneWARctiNINGon : Targefailed. t conneGDBServectr will beion los closet.
  d...Restoring target state and closing J-Link connection...
  Shutting down...
  Could not connect to target.
  Please check power, connection and settings.

Tried on Mac OSX and it also does not work probably for other reasons.

0 Kudos
Reply

16,170 Views
BlackNight
NXP Employee
NXP Employee

Hi Marcelo,

I have seen things like that if using different IDEs with using different Segger J-Link DLLs. I suggest you run

C:\Program Files (x86)\SEGGER\JLink_V620g\JLinkDLLUpdater.exe

and make sure all IDEs are using the same version of the Segger runtime libraries.

I hope this helps,

Erich

0 Kudos
Reply

16,170 Views
BlackNight
NXP Employee
NXP Employee

I see that you are already using V6.20h of the Segger software. I'm using V6.20g and have not seen something like this, so it could be that this is because of that new version? If this problem did not occur with an earlier version, I would downgrade the Segger version to say V6.20g to single out that possible reason.

I hope this helps,

Erich

0 Kudos
Reply

16,170 Views
Designer11
Contributor IV

Hi Erich,

Thank you for your suggestion, I will install an older version of Segger software. Do I need to modify my computer firewall or antivirus software to allow certain ports or IP to go through? Or is there an issue with my hardware? 

Thanks,

Vu

0 Kudos
Reply

16,170 Views
BlackNight
NXP Employee
NXP Employee

Hi Vu,

Firewalls and virus scanners are always a concern, but I don't thin this is the case.

I see that you have specified a USB port in the segger configuration which is not really necessary (it will ask you if you have multiple probes connected). What is strange that it does not work for you with the P&E connection too. So this means either you have a fundamental problem with your host PC.

After re-reading things, I'm puzzled what you mean by 'reset my computer'?

I hope this helps,

Erich

0 Kudos
Reply

16,170 Views
Designer11
Contributor IV

Hi Erich,

Thank you very much for your replies. I just finished downloaded and installed Segger software version 6.20g on my computer. However, the  SEGGER GDB Software GUI still refuses to establish connection with the GDB server. On the other hand,  this morning KDS decided to connect to the GDB server and i'm able to debug my code at the moment.

You mentioned about potential fundamental problems with my host computer. What kind of issues should i look into ?

BR,

Vu

0 Kudos
Reply