JTAG interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG interface

1,835件の閲覧回数
lifeng
Contributor II

pastedImage_1.png

The above picture is the jatg interface in  TWR-KE18F.

 

The jlink_jtag interface (10 pin) is pastedImage_2.png

They are different,  why?

0 件の賞賛
返信
2 返答(返信)

1,616件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Li Feng,

Which j-link adapter are you using? The J-Link 9-pin Cortex-M Adapter has the following pinout:

J-Link_9-pin_Cortex-M_Adapter.png

Here is more detailed information:

9-Pin Cortex M Adapter | SEGGER - The Embedded Experts 

Best Regards!
Carlos Mendoza
Technical Support Engineer

1,616件の閲覧回数
lifeng
Contributor II

Think you!

0 件の賞賛
返信