JLINK Debugger variable content view not shown

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JLINK Debugger variable content view not shown

1,069件の閲覧回数
michaelheidinge
Contributor III

Hello,

 

when debugging with the Kinetis K22F i used openOCD. When I go there with my mouse pointer over the variable view, the content of the variables is displayed.

 

Now I needed to switch to JLInk as I want to use my custom board, and if I hover now over the variables in the debug view - no variable content is displayed.

 

How Do I get that the variable contents are displayed using KDS 3.2 and Segger JLink?

 

-Michael

ラベル(1)
0 件の賞賛
返信
1 返信

971件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Michael,

In KDS , you can use the  "Expressions view"  to view variable :

pastedImage_0.png

you can open this view at the Window :

pastedImage_1.png

And also when you put the mouse point over the variable ,it also can show the data 。

Hope it helps

Alice

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信