JLINK Debugger variable content view not shown

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JLINK Debugger variable content view not shown

1,078 Views
michaelheidinge
Contributor III

Hello,

 

when debugging with the Kinetis K22F i used openOCD. When I go there with my mouse pointer over the variable view, the content of the variables is displayed.

 

Now I needed to switch to JLInk as I want to use my custom board, and if I hover now over the variables in the debug view - no variable content is displayed.

 

How Do I get that the variable contents are displayed using KDS 3.2 and Segger JLink?

 

-Michael

Labels (1)
0 Kudos
Reply
1 Reply

980 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Michael,

In KDS , you can use the  "Expressions view"  to view variable :

pastedImage_0.png

you can open this view at the Window :

pastedImage_1.png

And also when you put the mouse point over the variable ,it also can show the data 。

Hope it helps

Alice

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply