Issue getting KDS 1.1.0 to debug FRDM-KL02Z board using PE_Micro/OPENSDA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue getting KDS 1.1.0 to debug FRDM-KL02Z board using PE_Micro/OPENSDA

1,772 次查看
Pirosity
Contributor I

I'm having an issue getting my FRDM-KL02Z board communicating to KDS 1.1.0


I've installed the openSDA application DEBUG-APP_v105_Pemicro.SDA provided in the FRDM-KL02Z_QSP within the FRDM-KL02Z board.  I get a solid green light on the board and and I can connect to the board using code-warrior 10.4. 

 

I've verfied that the USB drivers for the PE micro openSDA debugger are present in device manager:

13908_13908.jpgdevice manager.jpg

 

Here is the debug configuration I setup:

13909_13909.jpgdebug screen.jpg

When i hit the debug button i get the following error message:

13911_13911.jpgerror message.jpg

Any idea what this error message means?

标签 (1)
0 项奖励
回复
2 回复数

1,489 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

not sure if this matters, but:

P&E has an updated debug app (MSD-DEBUG-FRDM-KE02Z_Pemicro_v114.sda), available from https://www.pemicro.com/opensda/.

At least this is what I'm using.

And with this I can debug my board. Your settings in the screenshots looks good to.

Just in case, I have attached my project. Note that I had to increase the heap size in the linker file because the newlib-nano needs that.

Can you try this?

I hope this helps,

Erich

0 项奖励
回复

1,489 次查看
cesarrabak
Contributor III

By the same token of lateral pertinency  :smileyhappy:, it may help to remember that in version 1.1.1 of KDS in the pemicro\opensda folder under the KDS 1.1.1 installation folder it can be found all the updates for SDA from P&E.

HTH

--

Cesar Rabak

0 项奖励
回复