Is KDS compatible with Eclipse Luna?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is KDS compatible with Eclipse Luna?

Jump to solution
2,058 Views
davepfaltzgraff
Senior Contributor I

For an unrelated project, I've installed the Luna release of Eclipse. This leads to several questions:

 

1. Can I run the KDS in Luna?

 

2. If so is the installation of KDS any different?

 

3. If not, can the Luna and Eclipse releases coexist?

 

Thanks

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,872 Views
BlackNight
NXP Employee
NXP Employee

1. No. KDS comes with its own Eclipse (Kepler) and is tested with it.

2. See 1. Because the Processor Expert plugin and components do not run in Luna (yet).

3. Yes.

Erich

View solution in original post

0 Kudos
Reply
1 Reply
1,873 Views
BlackNight
NXP Employee
NXP Employee

1. No. KDS comes with its own Eclipse (Kepler) and is tested with it.

2. See 1. Because the Processor Expert plugin and components do not run in Luna (yet).

3. Yes.

Erich

0 Kudos
Reply