Is CDT Build Console the same as the gdb (arm-none-eabi) console?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is CDT Build Console the same as the gdb (arm-none-eabi) console?

1,681 Views
christopherira
Contributor III

Hi,

 

I'm following a tutorial on mcuoneclipse and they use gdb (arm-none-eabi) console.

In Kinetis Design Studio I only have CDT Build Console and CDT Global Build Console. Will these work the same way?

 

Thanks,

 

Chris

Labels (1)
0 Kudos
Reply
2 Replies

1,565 Views
BlackNight
NXP Employee
NXP Employee

Hi Christopher,

in Eclipse, each subsystem can define and use its own 'sub console' for output. For the build (make) system, the two consoles you mention are used. The GDB consoles only show up when you start a debug sessions.

Erich

0 Kudos
Reply

1,565 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

The CDT debugger uses GDB as the underlying debug engine. It translates each user interface action into a sequence of GDB commands and processes the output from GDB to display the current state of the program being debugged.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply