Hi,
Ive checked the memory and memory browser tab while debugging my code. Also ive noticed that after bulding my app it dis show up some memory distribution of the controller in the console. But after after the second time build it wont show the same. It would be great to see a graphical representation for the same. Is there any option for that???
Regards,
Nelson Lobo
解決済! 解決策の投稿を見る。
Hi Nelson,
bss is uninitialized data, see text, data and bss: Code and Data Size Explained
I hope this helps,
Erich
Hello Lobo,
Please check "print size", then build , the code size will show on the console view :
And it seems there isn't graphical representation for the same .
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alice,
I already have that option enabled which provides the following:
'Invoking: Cross ARM GNU Print Size'
arm-none-eabi-size --format=berkeley "1.gpio_setup.elf"
text data bss dec hex filename
12100 188 2116 14404 3844 1.gpio_setup.elf
'Finished building: 1.gpio_setup.siz'
As per my understanding:
text : program/flash memory
data: static ram
bss : ??? (assuming the MCU registers)
is that right??? if not please do correct me.
Regards,
Nelson Lobo
Hi Nelson,
bss is uninitialized data, see text, data and bss: Code and Data Size Explained
I hope this helps,
Erich