How to view Kinetis ADC register in KDS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to view Kinetis ADC register in KDS?

1,009件の閲覧回数
wangbaode
Contributor IV

Dear all,

I want to view Kinetis ADC register in KDS.but I just find CPU register.How to view Kinetis ADC register in KDS?

 

bye

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

691件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

there is an open source Eclipse plugin you can download and install, see

How to Add Register Details View in Eclipse | MCU on Eclipse

Then add the Freescale CMSIS-SVD files and patch which is available on SourceForge:

Updated Eclipse EmbSysReg Viewer with extra Freescale SVD Files | MCU on Eclipse

The patch is available here:

McuOnEclipse - Browse /Eclipse Plugins/EmbSysReg at SourceForge.net

Regards,

Erich

0 件の賞賛
返信