How to use DMA and SPI components with processor expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use DMA and SPI components with processor expert

1,969 次查看
hengwu
Contributor I

I met a problem  when i use DMA and SPI components

 

I add a  fsl_dspi component which came up with a  referenced component called fsl_dma.

 

But I can not find configurations such as source address , destination address in the component of fsl_dma .

 

However in the component  Init_eDMA , I can find these configurations.

 

When i add Init_eDMA ,it occurred an error as follow lists.

 

31467_31467.pngpastedImage_0.png31468_31468.pngpastedImage_1.png

 

How should I add components and use when i want use spi and dma .

 

So if someone knows, please ...

标签 (1)
0 项奖励
回复
4 回复数

1,516 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Heng ,

(1) You can do like this :Delete the "fsl_edma" from your project , then configure the "Init_eDMA" .

(2) If it still can not meet your requirements, please provide these information : KDS and SDK version , and the chip name .


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,516 次查看
hengwu
Contributor I

Hi

if  I remove the fsl_dma, it occurred an error in the shared components of fsl_spi.

KDS is 2.0,SDK version is 1.2,the chip is mk64Fx512VLL12 .

Another problem is I just can not find the fsl_crc.

0 项奖励
回复

1,516 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello heng,

Sorry to reply you so late late .....

Have you problem been solved ?

If not , please create a new project ,then add the component "Init_eDMA" . I have test on my side , it can work well , my KDS is 3.0 , i think is the same with 2.0 .

pastedImage_0.png

If it still have error ,please send your project to me .

And i kindly recommend you use the latest version KDS 3.0, you can download here :

https://freescale.flexnetoperations.com/control/frse/product?entitlementId=123588587&lineNum=1&authC...


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,516 次查看
hengwu
Contributor I

Thanks a lot

0 项奖励
回复