How to initialize the DAC to start a conversion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to initialize the DAC to start a conversion

ソリューションへジャンプ
2,335件の閲覧回数
axl
Contributor I

Hi,

 

we are testing the audio processing capabilities of the K70 Tower.

 

We've been trying to configure the DAC through the Processor Expert interface. We've used the Kinetis/DAC_LDD component, with the hardware buffer disabled and without DMA.

The converted value seems to be stored in the internal registers but when we try to measure the output pin its value is different from the one we expect.

 

Would you know how to start the conversion and retrieve the converted value?

 

Please share your thoughts about this.

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,875件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Axel,

I'm guessing you need to select the clock source in the DAC_LDD component to be external.

Attached is my example project for TWR-K70F120M using KDS_3.0+KSDK_1.3+K70+PE+DAC_LDD using o-scope on J16-pin 1 (make sure jumper is removed).

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,876件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Axel,

I'm guessing you need to select the clock source in the DAC_LDD component to be external.

Attached is my example project for TWR-K70F120M using KDS_3.0+KSDK_1.3+K70+PE+DAC_LDD using o-scope on J16-pin 1 (make sure jumper is removed).

Regards,

David

0 件の賞賛
返信