How to add linked files in KDS V1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add linked files in KDS V1.1

Jump to solution
1,654 Views
randylee
Contributor V

IN CW 10.5 just under the import/exprort items in the context menus of the project or source directory, there is an "add files" which is where I can simply add files to the project and link files that I want noticed from elsewhere.

 

In KDS V1.1 There is no such option only import file file system and that doesn't let you link the file (i.e. just include it in the project without messing with it).

 

I see linked files in projects typically in the directory "Static_Code" so I know Elclipse hasn't forgotten how to do it, but I can't for the life of me find the majical incantation to just have it do it.

 

Any hints?

Labels (1)
0 Kudos
Reply
1 Solution
1,181 Views
BlackNight
NXP Employee
NXP Employee

Here are multiple ways and hints:

Link to Files and Folders in Eclipse | MCU on Eclipse

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
2 Replies
1,181 Views
randylee
Contributor V

yep, that got it.... thanx!

0 Kudos
Reply
1,182 Views
BlackNight
NXP Employee
NXP Employee

Here are multiple ways and hints:

Link to Files and Folders in Eclipse | MCU on Eclipse

I hope this helps,

Erich

0 Kudos
Reply