How to add device in KDS3.0 Embsys register viewer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add device in KDS3.0 Embsys register viewer

ソリューションへジャンプ
1,950件の閲覧回数
davidchen-b3693
NXP Employee
NXP Employee

Hi Sir :

         There are many Kinetis device can not be found in KDS3.0 Embsys register viewer . For example , KE , KM , KV3 , KV4 .... series . 

Is there any update to add those device in register viewer  ?

Thanks .

 

David 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,365件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

please make use you have all KDS updates installed.

if still can't find the missing device,

please unzip attached package and copy the content into your KDS embsysregview install folder

C:\Freescale\KDS_3.0.0\eclipse\plugins\org.eclipse.cdt.embsysregview.data_0.2.4.freescale\data\SVD(CMSIS)\Freescale

there is 107 devices included, KE , KM , KV3 , KV4 .... series are also included.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,365件の閲覧回数
davidchen-b3693
NXP Employee
NXP Employee

Hi Zhang Jun and Erich :

     Much thanks for your kindly support .

I found the issue why my KDS3.0 miss so many Freescale device .

There are two embsysregview in my KDS folder , one is Ver 0.2.4 another is 0.2.5.r180 .

I checked "Freescale " folder in those embsysregview folder .

Ver0.2.4 support a lot of Freescale Kinetis device .

Ver 0.2.5.r180 only support a little standard parts .

registerview1.JPGregisterview2.JPG

However , Ver 0.2.5.r180 embsysregview is engaged in my KDS3.0 , so many Kinetis device are missed .

Now I copy Jun's attach file to 0.2.5.r180 folder , and it works .

Thanks again .

David

0 件の賞賛
返信
1,365件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The EmbSysRegView uses normal SVD files (with .xml extension).

These are the ones which come with KDS v3.0.0:

pastedImage_0.png

The files are inside

C:\Freescale\KDS_3.0.0\eclipse\plugins\org.eclipse.cdt.embsysregview.data_0.2.4.freescale\data\SVD(CMSIS)\Freescale

pastedImage_1.png

I hope this helps,

Erich

0 件の賞賛
返信
1,366件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

please make use you have all KDS updates installed.

if still can't find the missing device,

please unzip attached package and copy the content into your KDS embsysregview install folder

C:\Freescale\KDS_3.0.0\eclipse\plugins\org.eclipse.cdt.embsysregview.data_0.2.4.freescale\data\SVD(CMSIS)\Freescale

there is 107 devices included, KE , KM , KV3 , KV4 .... series are also included.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信