How to add a board to Kinetis Design Studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to add a board to Kinetis Design Studio

跳至解决方案
2,642 次查看
eduardoumana
Contributor III

When I create a new "Kinetis Design Studio Project," only the K64F board is listed. How can I add the K22F board, which I am using, to Kinetis Design Studio?

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,869 次查看
BlackNight
NXP Employee
NXP Employee

Hi Eduardo,

Boards and new devices are added to KDS with the Kinetis SDK.

So download the K22F Kinetis SDK (SDK V1.0.0) from www.freescale.com/ksdk, then install it.

Use in KDS the menu Help > Install New software and use the zip file from

C:\Freescale\KSDK_1.0.0\tools\eclipse_update

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,869 次查看
jverive
Contributor III

Eduardo,

Also remember to follow instructions for building the platform driver library (see the appropriate section in the Kinetis SDK K22 User's Guide). You may already have been aware of this, but it was a huge source of frustration to me getting started with my K22F board.

Jeff

0 项奖励
回复
1,870 次查看
BlackNight
NXP Employee
NXP Employee

Hi Eduardo,

Boards and new devices are added to KDS with the Kinetis SDK.

So download the K22F Kinetis SDK (SDK V1.0.0) from www.freescale.com/ksdk, then install it.

Use in KDS the menu Help > Install New software and use the zip file from

C:\Freescale\KSDK_1.0.0\tools\eclipse_update

I hope this helps,

Erich

0 项奖励
回复
1,869 次查看
carloshass
Contributor II

Erich,

The TRK-KEA Boards are not supported by KDS?

0 项奖励
回复