How to add a board to Kinetis Design Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add a board to Kinetis Design Studio

Jump to solution
2,741 Views
eduardoumana
Contributor III

When I create a new "Kinetis Design Studio Project," only the K64F board is listed. How can I add the K22F board, which I am using, to Kinetis Design Studio?

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
1,968 Views
BlackNight
NXP Employee
NXP Employee

Hi Eduardo,

Boards and new devices are added to KDS with the Kinetis SDK.

So download the K22F Kinetis SDK (SDK V1.0.0) from www.freescale.com/ksdk, then install it.

Use in KDS the menu Help > Install New software and use the zip file from

C:\Freescale\KSDK_1.0.0\tools\eclipse_update

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
3 Replies
1,968 Views
jverive
Contributor III

Eduardo,

Also remember to follow instructions for building the platform driver library (see the appropriate section in the Kinetis SDK K22 User's Guide). You may already have been aware of this, but it was a huge source of frustration to me getting started with my K22F board.

Jeff

0 Kudos
Reply
1,969 Views
BlackNight
NXP Employee
NXP Employee

Hi Eduardo,

Boards and new devices are added to KDS with the Kinetis SDK.

So download the K22F Kinetis SDK (SDK V1.0.0) from www.freescale.com/ksdk, then install it.

Use in KDS the menu Help > Install New software and use the zip file from

C:\Freescale\KSDK_1.0.0\tools\eclipse_update

I hope this helps,

Erich

0 Kudos
Reply
1,968 Views
carloshass
Contributor II

Erich,

The TRK-KEA Boards are not supported by KDS?

0 Kudos
Reply