Hi Alice,
Thanks for your reply.
Yes we need to run from flash.
Actually we built a custom board using KL17Z controller and working on
developing the application code for a DC - DC converter.
The code functions as expected in debug mode as well as immediately after
flashing the code & if not power cycled.
But in standalone mode, the controller starts functioning only if we do the
hard reset (resetb port) the controller. I don't know why the controller
needs hard reset. we are using RC (10K & 0.1uF) circuit as recommended by
the NXP.
Plz help me to figure out a solution for this issue.
Thanks,
Muniraj
On Wed, Aug 31, 2016 at 9:07 AM, Alice_Yang <admin@community.freescale.com>