How do you display port and module registers in Kinetis Design Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do you display port and module registers in Kinetis Design Studio

1,997 Views
Kenm
Contributor II

How do you display port and module registers in Kinetis Design Studio?  So they can be changed

Are these registers in the configuration registers?

Labels (1)
0 Kudos
Reply
3 Replies

1,758 Views
BlackNight
NXP Employee
NXP Employee

Hi Ken,

you need to install an additional plugin.

See

http://mcuoneclipse.com/2014/05/29/how-to-add-register-details-view-in-eclipse/

Then apply the V0.3 patch from SourceForge which has the Freescale CMSIS-SVD files in it from McuOnEclipse - Browse /Eclipse Plugins/EmbSysReg at SourceForge.net

I hope this helps,

Erich

0 Kudos
Reply

1,758 Views
jinxin_cn
Contributor I

Hi Erich,

I can't find the chip KV31F51212 in V0.4 patch. How could I do?

B.R.

Jin Xin

0 Kudos
Reply

1,758 Views
BlackNight
NXP Employee
NXP Employee

You could use the files from Kinetis Design Studio v3.0.0:

pastedImage_0.png

?

Erich