Help to import Connectivity Software examples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help to import Connectivity Software examples

1,106 Views
marcolotz
Contributor I

Hello,
I have installed the Connectivity Software Tool to use the MKW40 BLE, after,  i builded
the ksdk_platform_lib_KW40Z4 on the Kinetis Studio IDE then the libksdk_plataform.a file
was created but yet i cant import any MKW40 examples(like the ones that comes with
Connectivity Software or the Zumobot example).
Could someone what i can do ? or show some tutorial link to how setup Kinetis Studio 3.2 for MKW40 ?
Using Kinetis Studio 3.2 and  KSDK1.3.0
Many Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,020 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Marco

I recommend you use the latest version of "Kinetis Connectivity Software Version 1.0.2 ",

this is based on KSDKv2.0, so after download and install it , do not need build any lib , we can

directly import the demo as these steps :

pastedImage_2.png

pastedImage_1.png

select the demo you need :

pastedImage_3.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply