Heap and Dynamic Memory Allocation on K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Heap and Dynamic Memory Allocation on K64F

3,484件の閲覧回数
torquatocecchin
Contributor I

Hi, I'm using FRDM-K64F dev board and I would like to use the the Heap for large array data allocation.

I tried suggested settings for heap and stack in PE (like changing heap and stack in the PEx CPU Build panel) with no compiling errors but failing debugging at run time.

I would like to configure the heap  for using .data sections areas and allow malloc() to dynamically allocate arrays in this area.

I don't use any ROTS since I prefer bare metal configurations and programming with KDS and PEx without KSDK.

A user heap section specification like possible with FreeRTOS would be perfect but I don't know how to do it without.

Thank you for your help guys.

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,597件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Torquato,

Could you please show your configuration and code , and i will test on my side .

BR

Alice

0 件の賞賛
返信

2,597件の閲覧回数
torquatocecchin
Contributor I

Hi Alice.

Thanks for your the interest.

I kept the standard memory sections  config.

I tried changing the in the Build Options settings panel:

pastedImage_0.png

the Heap amount from 0x0400 to upper values (0x0C00 or 0x1000) with no compiling and linking errors, but I have run time exceptions on isatty() call.

Following suggestions like described in Memory Areas and Using malloc() , I tried to configure linker with -WI switch but I think that symbol definition is different from the one I used. I found other suggestions like reported in compiler construction - use no heap in gnu gcc - Stack Overflow  and others without achieving more heap.

I'm testing the available memory amount with this simple function

uint32_t GetAvailableMemory(void)

{

  char *p;

  uint32_t siz = 1;

  p = calloc(1,siz);

  while (p)

      {

       siz++;

       p = realloc(p,siz);

       }

  free(p);

  return siz;

}

At least I could follow tweaks like Allocation of Variables at Absolute Address in RAM - Cypress using static or global pre-allocation

but I would like not to change malloc()-like calls because I'm generating C-code from a Matlab algorithm.

The .ld Linker file obviously reflects the PE config for I ask to generate linker code.

0 件の賞賛
返信

2,597件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Torquato,

I test your code on my side , the realloc() function can work well,  while i don/t know why you use while(p) , does here the "P"can repeated by some other

cycle conditons?

And i'm sorry that i don't know where you think is wrong , could your  tell me ? and tell me the right situation you think ! thank !

BR

Alice

0 件の賞賛
返信