Having difficulty loading program into evaluation board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Having difficulty loading program into evaluation board

3,331件の閲覧回数
mark_bresler
Contributor I

Hi,

I am using a Macintosh computer running KDS 3.0.0 and SDK 1.2.0. I have watched the video by Jorge_Gonzalez #3195 about 100 times (if not more) and have completed his example. I am having trouble downloading the code to the FRDM-K64F evaluation board. Using the Debugger, I get the following error alert:

 

J-Link GDB Server failed:

Could not connect to J-Link. Please check if plugged into USB port or Ethernet switch.

 

For more details, see the JLinkGDBServerCL console.

 

When I try to load

JLink_OpenSDA_V2_2015-06-11.bin into the bootloader virtual disk, the desktop computer gives an alert that the disk was not ejected properly, and the green LED to blink fast.  Disconnecting the USB cable from the SDA port, reconnecting the cable and pressing reset causes the green LED to blink slowly.   

 

Is there a tutorial or video I can use to work through this process?

Thanks,

Mark                      

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,273件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Mark,

It looks you don´t have correctly set debugger for J-Link.

Please, can you show us your Debug Configurations?

Also very useful tutorial for you can be :

Video Link : 3283

Best Regards,

Iva

0 件の賞賛
返信

2,273件の閲覧回数
mark_bresler
Contributor I

Iva,

Thanks for offering to look over my configuration settings. How can I show them to you, there are many tabs and click boxes? Are some more important than others?

Thanks,

Mark

0 件の賞賛
返信

2,273件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Mark,

it looks you are still  in  bootloader more.

Please, do you have correctly set J-link for you device?

  • Loading firmware

1. Unplug the USB cable (if attached).

2. Press and hold the Reset button.

3. Plug in a USB cable from a USB Host to the OpenSDA USB port.

4. Release the RESET/Bootloader button.

  • J-link in Device Manager

Please, just for information, take a look at Device Manager if you see J-link in Ports.

port.png

Here is tutorial how to sett up J-Link firmware Segger J-Link Firmware for OpenSDAv2 | MCU on Eclipse

Please, let me know if it helps you.

Best Regards,

Iva

0 件の賞賛
返信