GDB server fails to start

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GDB server fails to start

ソリューションへジャンプ
5,561件の閲覧回数
stevescott
Contributor II

Target is FRDM-KL27Z .

Running on Windows 7, 64-bit

Kinetis Design Studio, Version: 3.2.0

GNU ARM PEMicro Interface Debugging Support 2.6.0.201610062322

 

Trying to launch debugger using OpenSDA USB, I get an error:

 

166175_166175.pngpastedImage_2.png

 

Followed by:

 

166176_166176.pngpastedImage_3.png

 

 

I'm not sure if it's a hardware problem with my target board or an installation problem with the SDK, or other...???

 

Any help/feedback would be appreciated.

 

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
4,712件の閲覧回数
stevescott
Contributor II

This was a hardware issue. Several jumpers (J5,J6,andJ7) were missing. These jumpers isolated the OpenSDA USB from the MCU. The host could still see the OpenSDA processor, but couldn't get to the MCU. The gdb server launch failure was just a side effect.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,713件の閲覧回数
stevescott
Contributor II

This was a hardware issue. Several jumpers (J5,J6,andJ7) were missing. These jumpers isolated the OpenSDA USB from the MCU. The host could still see the OpenSDA processor, but couldn't get to the MCU. The gdb server launch failure was just a side effect.

0 件の賞賛
返信
4,712件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Have you checked if there is not another instance of the P&E GDB server running? See https://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/  and https://mcuoneclipse.com/2015/05/18/gdb-client-and-server-unlocking-gdb/ .

I hope this helps,

Erich

0 件の賞賛
返信
4,712件の閲覧回数
stevescott
Contributor II

Yes. There is no other copy of the server running. It appears to be a misleading error message. I think the real problem is not being able to connect to the target. 

0 件の賞賛
返信