Freemaster error in KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster error in KDS

1,083 Views
Lurkersoo
Contributor III

Hello, I try to use freemaster. I created a KDS project and compiled it. And then I opened the Freemaster, add the MAP file as below:

153401_153401.JPGfreemaster_Setting.JPG

And then an error occured:

153402_153402.JPGfreemaster_Error.JPG

It's very weird. I use CodeWarrior V10.6 created a project and compile, there are no this kind of error. Anybody can tell me why?

 

Best Regards,

Shaowei

Labels (1)
0 Kudos
Reply
1 Reply

967 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Shaowei,

Have you test the simple project ?

I create one simple project on the latest KDS v3.2 , then add the MAP file , there is no error.So could you please test other .elf file .

BR

Alice

0 Kudos
Reply