FreeRTOS OS abstraction component with KSDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS OS abstraction component with KSDK

1,320件の閲覧回数
Kewal
Contributor IV

I have configured the ethernet pins and debug UART pins and just have the os_abstraction component configured to freeRTOS.

 

When I add a project connection to the IAR and compile, I am getting an error which says me to include FreeRTOS.h before semphr.h and fortunately its been included in the only file fsl_os_abstraction_Free_rtos.h which is the only file which includes semphr.h

 

has anybody found success in using the os_abstraction component configured to freeRTOS earlier. is there anything which is missing and needs to be included manually.

 

Also very strangely, I found FreeRTOS.h(from FreeROTS itself), freeRTOS.h(generated by PE) and free_rtos.h(generated by PE).. for convienience i have added the snapshot, any help would be highly appreciated.74177_74177.JPGCapture.JPG

ラベル(1)
0 件の賞賛
返信
1 返信

1,159件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Kewal,

Jorge Gonzalez has already replied to your question on your thread under the KSDK community:

os_abstraction component +FreeRTOS

Let us know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信