FreeRTOS Clock_manager not installed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS Clock_manager not installed

ソリューションへジャンプ
5,763件の閲覧回数
EmanueleP
Contributor II

Hi,

i have a problem when i try to configure FreeRTOS in Kinetis Design Studio.

I'have installed Eclipse_add-on_to_add_FreeRTOS_Plug-ins-1.0.2.zip

and i have imported freeRTOS in my project (MCU is Kea128). In the configuration windows (in the figure) it can be see an error for clock_manager not installed. 

How can i solve?

Thanks

タグ(3)
0 件の賞賛
返信
1 解決策
5,757件の閲覧回数
ErichStyger
Specialist I

Hi @EmanueleP ,

I think the original NXP component does not support the KEA parts (I might be wrong). Anyway, I'm using the McuOnEclipse FreeRTOS component which does not have such a dependency on the clock manager:

https://mcuoneclipse.com/2021/12/26/mcuoneclipse-components-26-dec-2021-release/

I'm not developing anything on the KEA family (I had used the KE one), but if you want to consider that alternative FreeRTOS component, I could look into it.

 

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
5,758件の閲覧回数
ErichStyger
Specialist I

Hi @EmanueleP ,

I think the original NXP component does not support the KEA parts (I might be wrong). Anyway, I'm using the McuOnEclipse FreeRTOS component which does not have such a dependency on the clock manager:

https://mcuoneclipse.com/2021/12/26/mcuoneclipse-components-26-dec-2021-release/

I'm not developing anything on the KEA family (I had used the KE one), but if you want to consider that alternative FreeRTOS component, I could look into it.

 

I hope this helps,

Erich

0 件の賞賛
返信