FreeRTOS Clock_manager not installed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS Clock_manager not installed

Jump to solution
5,717 Views
EmanueleP
Contributor II

Hi,

i have a problem when i try to configure FreeRTOS in Kinetis Design Studio.

I'have installed Eclipse_add-on_to_add_FreeRTOS_Plug-ins-1.0.2.zip

and i have imported freeRTOS in my project (MCU is Kea128). In the configuration windows (in the figure) it can be see an error for clock_manager not installed. 

How can i solve?

Thanks

Tags (3)
0 Kudos
Reply
1 Solution
5,711 Views
ErichStyger
Specialist I

Hi @EmanueleP ,

I think the original NXP component does not support the KEA parts (I might be wrong). Anyway, I'm using the McuOnEclipse FreeRTOS component which does not have such a dependency on the clock manager:

https://mcuoneclipse.com/2021/12/26/mcuoneclipse-components-26-dec-2021-release/

I'm not developing anything on the KEA family (I had used the KE one), but if you want to consider that alternative FreeRTOS component, I could look into it.

 

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
1 Reply
5,712 Views
ErichStyger
Specialist I

Hi @EmanueleP ,

I think the original NXP component does not support the KEA parts (I might be wrong). Anyway, I'm using the McuOnEclipse FreeRTOS component which does not have such a dependency on the clock manager:

https://mcuoneclipse.com/2021/12/26/mcuoneclipse-components-26-dec-2021-release/

I'm not developing anything on the KEA family (I had used the KE one), but if you want to consider that alternative FreeRTOS component, I could look into it.

 

I hope this helps,

Erich

0 Kudos
Reply