Flashing KBOOT and Initial App

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing KBOOT and Initial App

ソリューションへジャンプ
2,434件の閲覧回数
alex323qp
Contributor III

Hi everyone, I'm trying to flash a custom bootloader based on the KBOOT 1.2 and also an initial app to my target KL25Z64 through KDS, using the PEMicro Universal Multilink FX. I'm first flashing the base app (with the right start location) and then the bootloader (.elf files), but it looks like on every flashing the previous binary gets replaced, is there any "right" procedure I'm not following?

 

p.s I also tried unchecking the "Mass erase on connect" checkbox without success.

107695_107695.pngpastedImage_0.png

 

Thanks in advance,

 

Alex.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,036件の閲覧回数
alex323qp
Contributor III

The answer was right under my nose:

For those that may have the same question, you can "Preserve" Memory ranges from the "Advanced Options" button.

More information here: preserved memory range problem in KDS 3.0

Cheers,

Alex.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,037件の閲覧回数
alex323qp
Contributor III

The answer was right under my nose:

For those that may have the same question, you can "Preserve" Memory ranges from the "Advanced Options" button.

More information here: preserved memory range problem in KDS 3.0

Cheers,

Alex.

0 件の賞賛
返信