Post port from CodeWarrior to KDS 2.0.0.
I get this when tiring to start a debugging session.
Error in final launch sequence
Failed to execute MI command:
tbreak main
Error message from debugger back end:
Cannot access memory at address 0x17bca
Cannot access memory at address 0x17bca
The only way I have found around this is to power on the K20 right before the code download begins.
Any thoughts on how to fix this?
SEGGER J-Link GDB Server V4.92 Command Line Version
JLinkARM.dll V4.92 (DLL compiled Sep 30 2014 09:33:42)
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: on
Silent mode: off
Single run mode: on
Target connection timeout: 5 sec.
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: MK20DN512xxx10
Target interface: JTAG
Target interface speed: 1000kHz
Target endian: little
Connecting to J-Link...
J-Link is connected.
Firmware: J-Link V9 compiled Sep 29 2014 18:56:38
Hardware: V9.00
S/N: 269301025
OEM: SEGGER-EDU
Feature(s): FlashBP, GDB
Checking target voltage...
Target voltage: 3.38 V
Listening on TCP/IP port 2331
Connecting to target...ERROR: Could not connect to target.
Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...
Shutting down...