FSL_Kinetis_Bootloader_1_2_0 loads, won't single step

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FSL_Kinetis_Bootloader_1_2_0 loads, won't single step

1,278 Views
colemanmoore
Contributor I

I am using the stand-alone Bootloader_1_2_0 with a custom MK22F25612 board.

 

I have programmed this to use the USB HID interface.

 

When starting a debug session, it stops at a breakpoint at main() prior to bootloader_init() as expected.

 

Giving the source debug area focus with the mouse or moving the mouse over the debug windows will cause the KDS title bar to display "not responding" and nothing will bring it out of that state except closing the KDS application.  KDS application restarts, re-powering the target board or resetting the computer (Windows 8)  do not help.

 

Any ideas?

 

Coleman

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,146 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Coleman,

Could you send us your project so we can test the issue on our side?

Thanks in advance.

Best Regards!

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply