FRDMK64 FTM2 Ch0 config problem with PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDMK64 FTM2 Ch0 config problem with PE

1,706件の閲覧回数
therealfreegeek
Contributor IV

Hi, I am using the FRDM K64 with KSDK1.3 and am trying to set up FTM2 Ch0 as an output but get an error from PE.

 

You can see from the image below I have selected the pin to be routed to J1-1 which is Port B18.

 

141823_141823.jpgftm2 A.jpg

 

I then try to select the pin direction as an output and get this error.

 

141860_141860.jpgftm2 B.jpg

 

Is this a bug or am I doing something wrong?

 

Thanks

Jim

ラベル(1)
3 返答(返信)

1,535件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello JIm,

I create one simple project to have a test , it can work well on my side,

and the attachment is my project ,you can test it on your side , it it can work well,

please create one simple project to have a try , or you can also send your project to me , i

will check it on my side .

pastedImage_0.png

Hope it helps

Alice

1,535件の閲覧回数
therealfreegeek
Contributor IV

Hi Alice,

Thanks for the offer, however I closed the project, removed it from the workspace and imported it again, the error then disappeared.

Thanks

Jim

0 件の賞賛
返信

1,535件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

OK Jim, welcome !

0 件の賞賛
返信