FRDM-KL26Z - Freedom Development Board Debugging issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-KL26Z - Freedom Development Board Debugging issue

1,301 次查看
dileeptn
Contributor I

Hi, 

Recently i bought a FRDM-KL26Z Freedom Development board. When i connected the board with mkl26z USB port with my pc, the drivers which required are installed. The RGB led ready to begin glow. RED BLUE etc at last it shows a combined color. The color will change with the motion of the board. Its works fine, and i tested the uart is working fine. Its display the value on my lap using teraterm. After that i updated the bootloader and firmware of the board,because i cant detect the port in KDS V3. Now KDS detect my board and port is also displayed. But the issue that the debugging is not completes. When i build the code (sampled code recommended in nxp - "hello world") no errors find and build complete. But when i debug it, the process stuck at about 75% completes. After that it doesnt moving what should i do? Is there is any issue with my over all work done? Or any issue with my KDS v3.

What is your suggestion? Any help will be appreciated.

Thanks 

Dileep

0 项奖励
回复
1 回复

1,192 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dileep ,

Please provde the below information:

- Which  bootloader and firmware you used ?

- What about your PC system ?

-Take a screesnshot about your Device manager  and Debug configuration of KDS when connect your board.

BR

Alice

0 项奖励
回复