FRDM K65 Board feasibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM K65 Board feasibility

1,873 Views
rahul_eris
Contributor II

Hi All,

 

We are planning to select Kinetis K65F board for our project development.

 

We need to implement all the below features on it.

   ---  Blue tooth and WIFI interfacing

   ---  Adding external  RAM memory to avoid memory concerns.

   ---  DHCP and IPV6 Implementation

 

Can anyone tell the feasibility of this board selection.

 

 

Which will be better module option for bluetooth, Wifi and external RAM interfacing in K65 family

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,722 Views
miduo
NXP Employee
NXP Employee

Hi,

It is feasible really! Even the K65 does not support BLE itself, but you can use the SPI to interface an external bluetooth chip. For Wifi connection, the K65 SDHC really compliance with the SDIO and can been used as WIFI communication. Also, we had the MQX RTCS really supporting thee DHCP and IPV6. Attached picture is a description for the hardware interface.

0 Kudos
Reply