FRDM K65 Board feasibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM K65 Board feasibility

1,874件の閲覧回数
rahul_eris
Contributor II

Hi All,

 

We are planning to select Kinetis K65F board for our project development.

 

We need to implement all the below features on it.

   ---  Blue tooth and WIFI interfacing

   ---  Adding external  RAM memory to avoid memory concerns.

   ---  DHCP and IPV6 Implementation

 

Can anyone tell the feasibility of this board selection.

 

 

Which will be better module option for bluetooth, Wifi and external RAM interfacing in K65 family

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,723件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

It is feasible really! Even the K65 does not support BLE itself, but you can use the SPI to interface an external bluetooth chip. For Wifi connection, the K65 SDHC really compliance with the SDIO and can been used as WIFI communication. Also, we had the MQX RTCS really supporting thee DHCP and IPV6. Attached picture is a description for the hardware interface.

0 件の賞賛
返信