Error while trying to update or install new software - KDS 3.2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error while trying to update or install new software - KDS 3.2.0

3,032 Views
armaram
Contributor III

I'm trying to install Embsysregview per instruction in the following link

How to Add Register Details View in Eclipse | MCU on Eclipse 

But for some reason keep getting the attached error (Cannot complete the request. This installation has not been configured properly for Software Updates.)

My software versions are the following
KDS Version: 3.2.0

Eclipse Version: Luna SR2 (4.4.2)

MCU: MKM34Z256XX5

Can anyone please help? 

I am trying to view the peripheral resisters after flashing my MCU. If there is any other way to view the peripheral register values kindly share those details.

Thank you.

Regards,

Arvind

2 Replies

2,818 Views
MarekTrmac
NXP Employee
NXP Employee

Hi Arvind,

the reason is KDS 3.2 already contains EmbSysRegView so it cannot be installed again.

Regards

Marek

0 Kudos
Reply

2,818 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Arvind,

KDSv3.2 can directly view the peripheral resisters with out any hesitate .

You can find it as below steps:

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------