Error in KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in KDS

904件の閲覧回数
donad
Contributor II

Hi,

When I run aprogram in KDS ,the following error shows up.

"The target endianness is set automatically (currently little endian) "

Why does this error occur? Please help.

 

Regards,

Dona

ラベル(1)
0 件の賞賛
返信
1 返信

824件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi dona,

can you shar a screenshot? I believe this is a message coming from the Segger J-Link debug firmware, and is not an error, but an information message. You can tell the Segger J-Link GDB server if it shall use little or big endian, and by default the firmware selects it automatically based on the device used, which is little endian for ARM.

I hope this helps,

Erich

0 件の賞賛
返信