Error Creating Segger Debug Config on KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error Creating Segger Debug Config on KDS

Jump to solution
2,280 Views
carloshass
Contributor II

I'm trying to change from PEMicro to Segger J-Link, but stuck imediatelly after clicking on GDB Server J-Link Debugging, for create the configuration for the Segger, and receiving following message:

 

93322_93322.pngpastedImage_0.png

 

Someone have some tip?

Labels (1)
0 Kudos
Reply
1 Solution
2,166 Views
BlackNight
NXP Employee
NXP Employee

Hi Carlos,

Have you updated the GNU ARM Eclipse plugins?

I think it is the same problem as described in Unable to Debug after KDS Update  (which has a patch as solution for it).

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
2 Replies
2,167 Views
BlackNight
NXP Employee
NXP Employee

Hi Carlos,

Have you updated the GNU ARM Eclipse plugins?

I think it is the same problem as described in Unable to Debug after KDS Update  (which has a patch as solution for it).

I hope this helps,

Erich

0 Kudos
Reply
2,166 Views
carloshass
Contributor II

i have 2 environments, one i've update, and another was fresh instalation of latest version.

And same error on both!

p.s.: Debug with pemicro is working(with a lot of "error setting bp"), then i'm trying to change to segger.

Boards is KE06Z.

Will try the link you provided and come back later.

0 Kudos
Reply