Download problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Download problem

1,222 次查看
mark_bresler
Contributor I

Hi,

Now that I have gotten my Bootloader problem solved ( Thank you Ping ), I have made a little progress, but am having a download problem.

I developed a program on my Macintosh computer ( a variant of the Red-Blue blink Carlos detailed in video 3195, to flash Red Green).

 

I get the following error message:

An error has occurred. See error log for more details.

ilg/gnuarmeclipse/debug/gdbjtag/data/CProjectAttributes

 

The Macintosh computer System Information program shows this information about the USB Bus and J-Link:

USB Bus:

 

  Host Controller Location: Built-in USB

  Host Controller Driver: AppleUSBOHCI

  PCI Device ID: 0x0aa5

  PCI Revision ID: 0x00b1

  PCI Vendor ID: 0x10de

  Bus Number: 0x04

 

J-Link:

 

  Product ID: 0x0105

  Vendor ID: 0x1366

  Version: 1.00

  Serial Number: 000621000000

  Speed: Up to 12 Mb/sec

  Manufacturer: SEGGER

  Location ID: 0x04100000 / 3

  Current Available (mA): 500

  Current Required (mA): 100

 

If someone can direct me on what to correct, it would be most appreciated,

Thanks,

Mark

标签 (1)
0 项奖励
回复
1 回复

1,071 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Mark,

do you use KDS3.0 or Codewarrior10.6?

if use KDS3.0, it can support  Mac OS 10.10 ("Yosemite").

Kinetis Design Studio Integrated Development |Freescale

if use CW10.6 it doesn't support Mac OS.

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复