Does anyone implemented HVAC using Kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does anyone implemented HVAC using Kinetis

1,201 Views
raveenmustala
Contributor I

Hello Everyone,

                Did anyone implement HVAC using kinetis Directly?

 

.

Labels (1)
0 Kudos
Reply
1 Reply

1,074 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Raveen Mustala,

On the Kinetis SDK v.1.2 you can find a demo application that demonstrates the Heating, Ventilating, and Air Conditioning demo on lwIP TCP/IP

stack with different RTOSes.

Here is the link to download the Kinetis software development kit:

Software Development Kit for Kinetis MCUs|Freescale

These Freescale Freedom development platforms and Tower System modules are supported by the Kinetis SDK web_hvac demo.

• FRDM-K64F

• TWR-K60D100M

• TWR-K64F120M

• TWR-K65F180M

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply