Disable clock in KSDK components

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disable clock in KSDK components

ソリューションへジャンプ
2,452件の閲覧回数
danielecortella
Contributor V

Hi all,

 

i'm using the sdks library but i have some problem with the clock source. In many components there isn't the possibility to disable the clock configuration. As is possible see in the picture the clock2 configuration that i use during the VLLS0 configuration go in conflict with the fsl_debug_console where i can't disable this clock configuration. Why this option is not enable in this new KSDK library? Thanks

 

Daniele

ラベル(1)
0 件の賞賛
返信
1 解決策
2,298件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Daniele Cortellazzi:

I think you are referring to a known issue in KSDK with Processor Expert. This is described in the Release Notes of the Eclipse Plugin for KSDK v1.1.0:

pastedImage_0.png

For now the workaround is to delete all conflicting clock configurations from the CPU component. You do not necessarily need to have only 1, there may be more than 1, as long as all of them can coexist with the components timings.

We know this is a limitation and you should be able to select the clock configurations you want. So this should be fixed with the next release of KSDK v1.2, available at the end of April.

Sorry for the inconvenience.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,299件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Daniele Cortellazzi:

I think you are referring to a known issue in KSDK with Processor Expert. This is described in the Release Notes of the Eclipse Plugin for KSDK v1.1.0:

pastedImage_0.png

For now the workaround is to delete all conflicting clock configurations from the CPU component. You do not necessarily need to have only 1, there may be more than 1, as long as all of them can coexist with the components timings.

We know this is a limitation and you should be able to select the clock configurations you want. So this should be fixed with the next release of KSDK v1.2, available at the end of April.

Sorry for the inconvenience.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,298件の閲覧回数
danielecortella
Contributor V

Thanks!

0 件の賞賛
返信