Disable PEx Static Driver Warning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disable PEx Static Driver Warning

ソリューションへジャンプ
3,068件の閲覧回数
jasonphilippi
Contributor III

Hello,

 

I am looking to disable the following warning in my project (GPIO):

 

Warning: This value is not available on this decive but is configurable in static driver. (Digital Filter)

Processor Expert Problem.

 

 

I don't see a warning number of sorts to disable it.

I don't want to disable all warnings, how can I disable just this warning?

 

Thank you,

 

Jason

ラベル(1)
0 件の賞賛
返信
1 解決策
2,775件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

Jason,

I think the message means, that selected pin does not support the feature, even it is configurable in the API.

The Processor Expert warnings cannot be disabled. It is possible to configure content of the Problems view (in Provlems view drop down menu - Configure Content ...).

Regards,Marek

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,775件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jason,

Which MCU are you using?

Could you tell post a screenshot of your workspace?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信
2,775件の閲覧回数
jasonphilippi
Contributor III

Hello Carlos,

I'm using KDS Version 3.0.0,  Processor Expert with KSDK 1.3 components, and a K24F .gpio-digital-filter.PNG

warnings.PNG

warning-settings.PNG

Let me know if you need any other relevant information.

Thank you,

Jason

0 件の賞賛
返信
2,776件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

Jason,

I think the message means, that selected pin does not support the feature, even it is configurable in the API.

The Processor Expert warnings cannot be disabled. It is possible to configure content of the Problems view (in Provlems view drop down menu - Configure Content ...).

Regards,Marek

0 件の賞賛
返信
2,775件の閲覧回数
jasonphilippi
Contributor III

Okay, this is what you are talking about, Help - Eclipse Platform.

  1. In Problems view, click the View Menu icon View Menu icon in the top right corner of the view.
  2. Use Configure Contents... to define your custom filter and click OK.
  3. In View Menu select Show and then your filter.

Thank you!

0 件の賞賛
返信