Differences in Debugging mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Differences in Debugging mode

2,071件の閲覧回数
matanhasan
Contributor I

hi!
I've got two computers with KDS on them, and trying to debug my MCU (MK10FN1M0VLQ12).

in one PC I've got the error : "Could not find core in Coresight setup",
and in the second one I've got the error: "Failed to unsecure Kinetis device".


I've checked the debug configurations in both of the computers, and found that they are the same, so i'm wandering what might be the problem.

thank you!

0 件の賞賛
返信
2 返答(返信)

1,706件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Matan Hasan,

It seems your chip is secured.

Which debug probe do you used ? Please unsecure it firstly.

BR

Alice

0 件の賞賛
返信

1,706件の閲覧回数
matanhasan
Contributor I

Yes, i tried that ->
secured & mass erase disabled Kinets MK10FN1M0XXX12 
this is a new thread.

0 件の賞賛
返信