Difference between the "Cross ARM C++ Compiler" and the "GNU ARM C++ Compiler"?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between the "Cross ARM C++ Compiler" and the "GNU ARM C++ Compiler"?

1,558 次查看
tharonhall
Contributor IV

It was suggested to me that the "Cross ARM C++ Compiler" is unique to KDS, and I should ask my question here:

 

Original Question:

 

What is the difference between the "Cross ARM C++ Compiler" and the "GNU ARM C++ Compiler"?

 

Is it a fork of the GNU? Does it support the same commands and pragmas as GNU?

 

I've had ZERO luck Googling this.

 

--------------------

Follow up Post:

 

I can note that since I posted this, I did see a comment somewhere that the Cross Compiler is derived from the GNU Compiler, but no explanation was given as to what the differences are.

 

标签 (1)
标记 (6)
0 项奖励
回复
0 回复数