Debug with starting address at 0x1000 instead of 0x0 in KL04z using PEMicro debugger on KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debug with starting address at 0x1000 instead of 0x0 in KL04z using PEMicro debugger on KDS

跳至解决方案
3,712 次查看
mjoa
Contributor II

Hi,


I have been using kinetis design tool to debug my code on microcontroller KL04z. Is there a way to run image with starting address at 0x1000 instead of 0x0 in KL04z on PEMicro debugger on KDS.

 

I have done the followings but in vain:

1. Change the following in MemoryMap-mkl04z32m4.ld to

  rom        (rx)  : ORIGIN = 0x1000, LENGTH = 0x7000

 

2. build the image

 

3a. On KDS, run PEMicro debugger => Not work. Stuck at 0xfffffffe

3b. On KDS, run PEMicro debugger, on runtime options setting PC to 0x1000 => not work. Stuck at 0xfffffffe.


Please see attached result.

18582_18582.pngstartaddress_not_0.PNG.png

 

Thanks a lot.

With regards,

Mario

标签 (1)
1 解答
3,203 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Mario:

I had no problems to debug from 0x1000 offset. Your description however mentions a section with name rom in the linker file. Is this an example project taken from some place? or did you create that project with KDS new project wizard?

For your reference I attach to this response the project I created moving code to 0x1000 address.

About the Flash Configuration Field, such information can be found in the Reference Manual in chapter 27.3.1 Flash Configuration Field Description and throughout other sections of the manual regarding security and booting options. You can also refer to AN4507 and AN4835.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
7 回复数
3,203 次查看
DavidS
NXP Employee
NXP Employee

Hi Mario,

Do you have a bootloader or other application to run at address 0x0?

Kinetis by default has the interrupt vector table at address 0x0 on Power On Reset (POR).

The address 0x00000000 has the stack address.  Initial Stack address points to internal SRAM (volatile memory).

The address 0x00000004 has the PC (Program Counter) address.  Initial PC points to flash (nonvolatile code) memory.

Also at address 0x400-0x410 are flash configuration fields that upon POR are read to determine the system permissions, security, boot methods, etc...  If these fields are not programmed correctly the device can be "bricked" (i.e. made inaccessible and must be replaced).  The most important field is the FSEC[SEC] field that should be binary 10 to keep the device in unsecure state to allow the debugger interface to operate.

In summary, code doesn't start at address 0x0.  That space is part of the vector table and the vector table addresses 0x0 and 0x4 have the stack and PC addresses that are fetched by the core on POR/reset to know where to start executing code.

Hope this helps.

Regards,

David

3,203 次查看
mjoa
Contributor II

Hi David,

Thanks for your reply.  I did not have a bootloader to run at address 0x0. I thought that PEMicro Multilink FX debugger could force KL04 to start from 0x1000 by setting start PC at 0x1000.

Previously, when using FRDM-KL05z as usbdm debugger, the image could run properly from 0x1000 even without bootloader at 0x0:Capture_usbdm.PNG.png 

So, I thought I could do the same on PEMicro  Multilink FX  debugger.  Probably, I am wrong.

BTW, I am new to KL04z. Where could I find the following information (such as application note) besides KL04 reference manual

"Also at address 0x400-0x410 are flash configuration fields that upon POR are read to determine the system permissions, security, boot methods, etc...  If these fields are not programmed correctly the device can be "bricked" (i.e. made inaccessible and must be replaced).  The most important field is the FSEC[SEC] field that should be binary 10 to keep the device in unsecure state to allow the debugger interface to operate."

Thank you so much

With regards,

Mario

0 项奖励
回复
3,204 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Mario:

I had no problems to debug from 0x1000 offset. Your description however mentions a section with name rom in the linker file. Is this an example project taken from some place? or did you create that project with KDS new project wizard?

For your reference I attach to this response the project I created moving code to 0x1000 address.

About the Flash Configuration Field, such information can be found in the Reference Manual in chapter 27.3.1 Flash Configuration Field Description and throughout other sections of the manual regarding security and booting options. You can also refer to AN4507 and AN4835.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,203 次查看
sumanmotaparthy
Contributor I

Hi Jorge,

               I do not find the attachment in your reply. Where can I get it? I am running into a similar issue where I want to debug code starting at 0x4000 instead of 0x0000 using PE Micro Universal Debugger. I am using a Kinetis K20 series of microcontroller.

Thanks and regards,

Suman

0 项奖励
回复
3,202 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Suman:

You are right, it seems I forgot the attachment, sorry. Now it is attached.

Regards!

Jorge Gonzalez

0 项奖励
回复
3,202 次查看
mjoa
Contributor II

Hi Jorge,

Sorry for delay. I have been pulled off to work on something else.

I have just tested your project. It works.

My project was created using USBDM tab on KDS. The structure as well as startup code in my usbdm-created project is quite different from yours.

Finally, the memory map is defined in ..\Project_Settings\Linker_Files\MemoryMap-mkl05z32m4.ld

The original setting is

MKL05Z32M4

*/

MEMORY

{

  ram        (rwx) : ORIGIN = 0x1FFFFC00, LENGTH = 0x00001000

  rom        (rx)  : ORIGIN = 0x00000000, LENGTH = 0x00008000

  io         (rwx) : ORIGIN = 0x40000000, LENGTH = 0x00080000

  io_1       (rwx) : ORIGIN = 0x400FF000, LENGTH = 0x00001000

  io_2       (rwx) : ORIGIN = 0x44000000, LENGTH = 0x1C000000

  io_3       (rwx) : ORIGIN = 0xE0000000, LENGTH = 0x00100000

  io_4       (rwx) : ORIGIN = 0xF0000000, LENGTH = 0x00001000

  io_5       (rwx) : ORIGIN = 0xF0001000, LENGTH = 0x00001000

  io_6       (rwx) : ORIGIN = 0xF0002000, LENGTH = 0x00001000

  io_7       (rwx) : ORIGIN = 0xF0003000, LENGTH = 0x00001000

  io_8       (rwx) : ORIGIN = 0xF8000000, LENGTH = 0x08000000

};

I have modified it into

MKL05Z32M4

*/

MEMORY

{

  ram        (rwx) : ORIGIN = 0x1FFFFC00, LENGTH = 0x00001000

  rom        (rx)  : ORIGIN = 0x00001000, LENGTH = 0x00007000 <= change

  io         (rwx) : ORIGIN = 0x40000000, LENGTH = 0x00080000

  io_1       (rwx) : ORIGIN = 0x400FF000, LENGTH = 0x00001000

  io_2       (rwx) : ORIGIN = 0x44000000, LENGTH = 0x1C000000

  io_3       (rwx) : ORIGIN = 0xE0000000, LENGTH = 0x00100000

  io_4       (rwx) : ORIGIN = 0xF0000000, LENGTH = 0x00001000

  io_5       (rwx) : ORIGIN = 0xF0001000, LENGTH = 0x00001000

  io_6       (rwx) : ORIGIN = 0xF0002000, LENGTH = 0x00001000

  io_7       (rwx) : ORIGIN = 0xF0003000, LENGTH = 0x00001000

  io_8       (rwx) : ORIGIN = 0xF8000000, LENGTH = 0x08000000

};

With regards

Mario

0 项奖励
回复
3,202 次查看
mjoa
Contributor II

Hi Jorge,

Thank you so much for your input

Mario

0 项奖励
回复