DATA_SEG with Kinetis development

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DATA_SEG with Kinetis development

Jump to solution
3,406 Views
iancull
Contributor III

My company has been using Freescale (HCS12X) parts for more than 10 years with CodeWarrior development.

 

We now want to use the Kinetis KE06Z part for a new lower code development. I have the FRDM-KE06Z board and have code running on it, using the CodeWarrior Development Studio V1.06. But as I progress I'm running into troubles.

 

My problem today started with the support or lack of support for #pragma. My research so far suggests there is NO SUPPORT for "#pragma DATA_SEG", for example. Is this true?

I want to place variables into specific memory locations so that both the normal project software, and the bootloader, can access the same data. How do I do this - in the past I used the DATA_SEG and then set up the linker to place that segment somewhere specific.

If no support for DATA_SEG, what is the alternative?

 

 

Documentation online is very confusing perhaps due to the Freescale / NXP business but also because there seems to be two separate development systems (the other is Kinetis Design Studio I think).

I wonder if I have chosen the wrong dev suite - where is any helpful information on which is the better choice, what the differences are, etc?

In any case does Kinetis Design Studio support "#pragma DATA_SEG"?

 

 

Thank you.

Ian Cull. PG Trionic Inc

Essex, MA, USA

Labels (1)
1 Solution
2,742 Views
BlackNight
NXP Employee
NXP Employee

Hi Ian,

things are a bit different in GNU/gcc/ld land. So yes, there is no such pragma CODE_SEG or DATA_SEG. Pragmas are very compiler specific.

But there is the very flexible __attribute__ in GNU land, e.g.:

static unsigned char __attribute__((section (".mySection"))) ucHeap[configTOTAL_HEAP_SIZE];

Additionally, you need to understand a bit the GNU linker file. Maybe have a look here which discusses a specific case how to allocate a variable in a special section:

FreeRTOS Heap with Segmented Kinetis K SRAM | MCU on Eclipse

Related on that topic, this might be helpful too: Defining Variables at Absolute Addresses with gcc | MCU on Eclipse

I hope this helps,

Erich

View solution in original post

4 Replies
2,743 Views
BlackNight
NXP Employee
NXP Employee

Hi Ian,

things are a bit different in GNU/gcc/ld land. So yes, there is no such pragma CODE_SEG or DATA_SEG. Pragmas are very compiler specific.

But there is the very flexible __attribute__ in GNU land, e.g.:

static unsigned char __attribute__((section (".mySection"))) ucHeap[configTOTAL_HEAP_SIZE];

Additionally, you need to understand a bit the GNU linker file. Maybe have a look here which discusses a specific case how to allocate a variable in a special section:

FreeRTOS Heap with Segmented Kinetis K SRAM | MCU on Eclipse

Related on that topic, this might be helpful too: Defining Variables at Absolute Addresses with gcc | MCU on Eclipse

I hope this helps,

Erich

2,742 Views
iancull
Contributor III

Many thanks, and fast! That "Defining Variables at Absolute Addresses with gcc" looks like it might be very much what I need, I'll try modifying my pragmas to match and see how it goes.

0 Kudos
Reply
2,742 Views
iancull
Contributor III

With that help, I'm done :smileyhappy:

In the linker file, I split off 16 bytes of memory:

MEMORY

{

  m_data      (rwx) : ORIGIN = 0x1FFFF800, LENGTH = 8K - 16 /* SRAM */

  m_fixedboot    (rwx) : ORIGIN = 0x200017F0, LENGTH = 16 /* SRAM */

}

And I set up a new section to fill it:

  .FIXEDBOOT_DATA :

  {

    *(.FIXEDBOOT_DATA1)

    *(.FIXEDBOOT_DATA2)

    *(.FIXEDBOOT_DATA3)

  } > m_fixedboot 

And in the memory definitions C code I labeled the variables (I did it this way in three section attributes since the order appeared unpredictable if I just put all in the same section):

byte __attribute__((section (".FIXEDBOOT_DATA1"))) ramFlashCodes[4];

byte __attribute__((section (".FIXEDBOOT_DATA2"))) ramResetData[4];

longword __attribute__((section (".FIXEDBOOT_DATA3"))) ramPowerUpCheck;

Perfect, thanks.

2,742 Views
Jiun_Yong
Contributor III

HI Ian

Like you, our company has used HSC12X for years and I am getting to grips with Kinetis for a new project (specifically the KL26).

As you noted, there is no direct equivalent of the #pragma DATA_SEG.

The downside of the method you have used is that you have to insert the __attribute__ ((section(".mydata"))) statement into every declaration for constants.

The alternative is to use the linker file to put all constant data from a given source file into the specified memory area as follows:

1. Put your constant data into a separate source file. In my project, it's called "changer_data.c"

It can be defined simply as "const byte ramFlashCodes[4];" etc.

2. in the MEMORY{} block define a segment of memory where the data will be stored.

E.g.   m_changer_data (R) : ORIGIN = 0x00003600, LENGTH = 0x00001000

3. In the SECTIONS{} segment, add a statement that directs all output from the source file with the constant data to this segment. E.g.

  .m_changer_data_seg :

  {

  . = ALIGN(4);

  *changer_data.o (.rodata .rodata*)

  . = ALIGN(4);

  } > m_changer_data

This will take all the compiled output from "changer_data.c" and link it into the m_changer_data area of memory.

I got this from another post by Eric Styger at Putting Code of Files into Special Section with the GNU Linker | MCU on Eclipse

Hope this helps