Connection Error using Multilink Universal with Kinetis MKV46F256VLL16 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connection Error using Multilink Universal with Kinetis MKV46F256VLL16 processor

Jump to solution
1,573 Views
boubacarhoussei
Contributor I

Hello,

I want to directly program the MKV46F256VLL16 processor on the TWR-KV46F150M board through a PEmicro USB-ML-Universal Interface. I got connection error when launching the Debug Configurations using KDS 3.2.0.

In debug configuration I use the following configuration:  GDB PEMicro Interface/USB Multilink, Port/USB1-Multilink Universal Rev B (PE5655394).

I appreciate your help.

Bouba
1 Solution
1,429 Views
boubacarhoussei
Contributor I

I get it working. It was hardware configuration issue. I opened jumpers J521 & J522 on the TWR-KV46F150M board and it works perfectly.

View solution in original post

1 Reply
1,430 Views
boubacarhoussei
Contributor I

I get it working. It was hardware configuration issue. I opened jumpers J521 & J522 on the TWR-KV46F150M board and it works perfectly.