Connection Error using Multilink Universal with Kinetis MKV46F256VLL16 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Connection Error using Multilink Universal with Kinetis MKV46F256VLL16 processor

跳至解决方案
1,616 次查看
boubacarhoussei
Contributor I

Hello,

I want to directly program the MKV46F256VLL16 processor on the TWR-KV46F150M board through a PEmicro USB-ML-Universal Interface. I got connection error when launching the Debug Configurations using KDS 3.2.0.

In debug configuration I use the following configuration:  GDB PEMicro Interface/USB Multilink, Port/USB1-Multilink Universal Rev B (PE5655394).

I appreciate your help.

Bouba
1 解答
1,472 次查看
boubacarhoussei
Contributor I

I get it working. It was hardware configuration issue. I opened jumpers J521 & J522 on the TWR-KV46F150M board and it works perfectly.

在原帖中查看解决方案

1 回复
1,473 次查看
boubacarhoussei
Contributor I

I get it working. It was hardware configuration issue. I opened jumpers J521 & J522 on the TWR-KV46F150M board and it works perfectly.