Can't get CAN reception interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't get CAN reception interrupt

1,241 Views
hanchengyang
Contributor II

Hello,

 

Recently I transmitted my work from CW 10.6 with KE06 to KDS with K64F, both with MQX Lite and PEx.

 

Firstly I would like to ask that I cannot get work with PEx, KSDK, because it said : "Processor Expert does not support KSDK 1.1.0-GA for board FRDM_K64F" when I try to create the project.

 

It's because the problem above that I continued to use MQXLite. I connected the CANRx and CANTx with externel CAN bus controller, I always can't enter the CAN reception interrupt with CAN transmission successful. In the loop mode I got the same result. Nothings received.

 

So please help me.

 

Thanks,

YANG Hancheng

Original Attachment has been moved to: EP_Tender_k64f.7z.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,009 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello YANG Hancheng,

KDS2.0 for K64F can support PEx and KSDK together. see attached video.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply