Build difference between KDS2.0 and KDS3.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Build difference between KDS2.0 and KDS3.0

跳至解决方案
2,153 次查看
yarannan
Contributor III

Hi,

I have an issue about building my project on KDS 3.0. Below is what happened:

1. I installed KDS3.0 to a new computer due to some work reason.

2. I check out the code from git.

3. Start build the project as i do usually but it throw error that says make*** [project.elf] Error 1

4. I ran different project and same thing happened. I decided to switch back to kds2.0

5. I uninstalled KDS3.0 and install KDS2.0. Import the project and build it. It succeed.

Therefore, here is what I wondered, is there any configuration that i have to do in order to run kds2.0 project

on KDS3.0?

 

Thanks,

 

Yaran

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,980 次查看
BlackNight
NXP Employee
NXP Employee

Hi Yaran,

What error have you received (Console view)?

Because KDS v3.0.0 is using the GNU ARM Embedded (launchpad) tools, you will need to migrate/change a linker setting. See Kinetis Design Studio: Migrating KDS V2.0.0 Projects to GNU Tools for ARM Embedded (Launchpad, KDS V...  for details.

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,981 次查看
BlackNight
NXP Employee
NXP Employee

Hi Yaran,

What error have you received (Console view)?

Because KDS v3.0.0 is using the GNU ARM Embedded (launchpad) tools, you will need to migrate/change a linker setting. See Kinetis Design Studio: Migrating KDS V2.0.0 Projects to GNU Tools for ARM Embedded (Launchpad, KDS V...  for details.

I hope this helps,

Erich

0 项奖励
回复