Hi,
I recently migrated my project from Code Warrior 11.1 to Kinetis Design Studio 3.2.0.
Previously, I used to flash a combined binary image of loader+bootloader+application_firmware into the MK10FX512VLQ12 MCU through the "Flash" option in Code Warrior 11.1 IDE. Currently, I'm using KDS for the same project, with the same MCU & created a combined binary image to flash from KDS. But, I get an error when I try to flash bin file from KDS 3.2.0 as "File format not recognised" which never happened in Code Warrior.
I have attached the error message screenshot below. Kindly help.
Regards,
Kritz