Kinetis デザインスタジオ・ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Design Studio Knowledge Base

ラベル

ディスカッション

ソート順:
Based on Erich's HID Mouse tutorial, this is a simple HID compliant Air Mouse, with the pointer being controlled using the onboard accelerometer.     A full Tutorial on how to make this project is available inside the Zip under "Simple Air Mouse on a FRDM KL25Z.pdf". It aims to fully explain the process of building the project in KDS, how to set up the board for HID interaction and how to setup the accelerometer.   Thanks go to Erich Styger for the original tutorial and insight, along with his incredibly handy component library.   If i've been confusing or have forgotten to note something (as I no doubt will have), please don't be afraid to message in to let me know and i'll update the relevant files.
記事全体を表示
NXP Touch software (http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m/kinetis-symbols-footprints-and-models/freescale-touch-software:FREESCALE-TOUCH-SOFTWARE ) is designed to speed development of your touch applications and is ideal for use with Kinetis MCUs. Because it is available as both a binary library and also in source code, many customers like using it.   Recently I received several cases from customers that some of our customers can’t run this package successfully. So I start to write this document of how to use this package to make this package “run” on your board!
記事全体を表示
Accelerometer in KDS Description:   This is a small project made in KDS using the accelerometer on a FRDM-MK64FN1M0VLL12 board. The blue LED is on when the board is flat or upside down The red LED is on when the board is on its side The green LED is on when the board is on its nose or tail   Sections of code taken from http://mcuoneclipse.com/2014/05/26/tutorial-data-logger-with-the-frdm-k64f-board/
記事全体を表示
Greetings, A new release V1.1.1 of KDS is available from the Download tab on http://www.freescale.com/kds V1.1.1 is a full release, and it is recommended to use this new release going forward. V1.1.1 supports Windows (7/8), Linux (32bit binaries for Ubuntu, RHE and CentOS): What's new: Linux RHE and CentOS installation (RPM) Updated KDS User Guide Updated P&E updated site handling to allow support for incremental device support Fixed IP Adddress Setup for P&E Ethernet connection devices (Cyclone MAX, TraceLink) For details, see the V1.1.1 Release Notes.   In addition to the KDS V1.1.1 release, there is an Eclipse update for Processor Expert and Kinetis SDK support. Implemented workaround for HEAP size needs of Newlib-nano GNU library Fixed include path delimiter for Linux hosts Fixed flash configuration field values for several bare project derivatives Updated board configuration templates. Details in the Update1 Release Notes.   Download this .zip file, then install it in Eclipse/KDS using the menu Help > Install New Software (the update will be available on the KDS Eclipse online update site too)   :   Please use KDS V1.1.1 with Eclipse/Processor Expert/SDK Update1 going forward. KDS V1.1.0 projects and settings can be used with V1.1.1.   Best regards, Erich
記事全体を表示
Writing to Acceleometer data to SD Card in KDS   Description:   A project made in KDS using the FRDM-MK64FN1MOVLL12 board to write the Accelerometer data to an SD Card. Every second, the time and the value of the variables x, y and z taken from the Accelerometer will be written to an SD Card. They will be written in a log.txt file, which will be created if it does not exist. The LED will flash green every second when writing. In case of an error, the LCD will flash red every second.   Sections of code taken from http://mcuoneclipse.com/2014/05/26/tutorial-data-logger-with-the-frdm-k64f-board/   Issues:   Time will always begin at 17:51:31 after being flashed. This is due to it being set as such at TmDt1_Init.
記事全体を表示
Temperature in KDS   Description:   A project made in KDS using the FRDM-MKL46Z256VLL4 board's LCD screen to display temperature. The LCD will display temperature data taken from the magnetometer in degrees Celsius. Data is read every 500ms as this lowers flickering when between temperatures.   Updates:   After initially submitting this project after having it working, I tried to load it up and found out the temperature not displaying correctly. After much trial and error I managed to find out that not initializing the magnetometer was causing the issues, even though it was not the previous day! Have edited the project to add in the initialization just in case it causes anyone else errors.
記事全体を表示
Taking code for a simple LCD function that is used in Code Warrior and modifying it for use in KDS on the FRDM-KL46Z board.
記事全体を表示
USB Mouse in KDS   Description:   A project made in KDS using the accelerometer on a FRDM-MKL46Z256VLL4 board to control a USB mouse input. A red LED will flash while not connected as a USB mouse, and green LED will flash when it is. SW1 will right click. SW3 will left click.   Sensitivity of the mouse can be changed by altering the HIDM1_Move command in main.c   Sections of code taken from: - http://mcuoneclipse.com/2012/09/21/tutorial-accelerating-the-kl25z-freedom-board/ - http://mcuoneclipse.com/2013/08/01/using-the-frdm-kl25z-as-a-usb-mouse-device/
記事全体を表示
For the Windows version of SDK, I was not able to use the OpenSDA with CMSIS-DAP running on the FRDM-KL25Z.. The Quick Start guide Figure 12 shows the a blank field for "Other options". You must enter "-f kinetis.cfg" here or you will not be able to debug. See below.
記事全体を表示
USB Keyboard in KDS   Description:   A project made in KDS using the FRDM-MKL46Z256VLL4 board as a USB keyboard input. A red LED will flash while not connected as a USB keyboard, and green LED will flash when it is. Switch SW3 will type 'SW3 Pressed' and switch SW1 will type 'SW1 Pressed' In Application.c is commented out example code for pressing print screen and control+alt+delete.   Sections of code taken from http://mcuoneclipse.com/2013/06/30/using-the-frdm-kl25z-as-usb-keyboard/
記事全体を表示
Light Intensity in KDS   Description:   A project made in KDS using the FRDM-MKL46Z256VLL4 board's LCD screen to display light intensity. The LCD will display light intensity taken from the light sensor.
記事全体を表示
In case you have created a project without Processor Expert option enabled at project creation time, it might be the easiest way just to create a new project with Processor Expert enabled, and then move things over. In case this approach is not feasible, then the following document outlines the steps to concert such a project into a Processor Expert project: Adding PEx to KDS bareboard project (with SDK) | Freescale Community   Happy Converting 🙂
記事全体を表示
hi, Thank you for your response. Now am sending the file in  .doc format please check it once and let me know where are the mistakes in porting. Thanks and Regards, Padmaja
記事全体を表示
This is an ISF2.1 Project that goes with the blog post titled "Creating a Data Logger embedded application using ISF 2.1".
記事全体を表示
This project is a re-build of Yayra Kwaku Adugu's E14 project, now built in KDS. The project allows the FRDM KL25Z to utilise an external E14 sensor board for accellerometer, magnetometer and pressure sensor, printing data to terminal.   Unfortunately this project runs afoul of a printf bug in KDS and not all printf calls will display properly. More information/examples of this bug can be seen at Re: printf() weirdness - Using printf() with ConsoleIO and TeraTerm via OpenSDA - issues   Hopefully if/when the printf implementation is fixed in KDS, the project should work fine and display data to terminal.   Project Info: Board used: MKL25Z128VLK4 Terminal Baud Rate: 9600
記事全体を表示